{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can you set up the ATV630 and ATV930 drive for sourcing or sinking logic inputs?

Issue:

ATV630 and ATV930 drive for sourcing or sinking mode?

Product Line:

ATV630 and ATV930 Family

Environment:

All

Cause:

Setting up the logic inputs to switch on with a sinking input to com.

Resolution:

The sink source switch is located on the face of the drive under the terminal IO block. Sink position is on the left and source position is on the right.

sink or source image I

Sink or Source image II

Schneider Electric Saudi Arabia