is it possible with EVlink Pro AC to change the max current or power depending on the time slot or tariff ?
Article available in these languages:Czech
Yes, by using the input current limitation or deferred start on the digital input of EVlink Pro AC. It is also possible to do this using EV Charging Expert or EV Advisor.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
EVlink Pro AC
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.