{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Some NBPD0165 cameras have motion mask on by default.
Issue:
Some NBPD0165 cameras have motion mask on by default.

Product Line:
NetBotz

Environment:
NBPD0165 camera

Cause:
Some NetBotz cameras may not be detecting motion due to a pre-set motion mask from the factory.

Resolution:
If your NetBotz camera pod NBPD0165 is not detecting motion when it clearly should be, simply turn off the motion mask using the following steps.

Log into the NetBotz Main appliance (750 or 755)
Select the camera pod by clicking on it on either the "Overview" page or the "Devices" page.
Click the "SETTINGS" button.
Below where it's marked "Draw on the camera image below to define regions where the camera will NOT detect motion." Click the "CLEAR ALL" button.
Scroll to the bottom of the page and click the "OK" button.

Specific to serial numbers starting in Jan 2022  ex.  9A2202Y01088
camera FW  a720211203NX

Schneider Electric Saudi Arabia