{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
"S_RD_ETH_MX2" is not working as expected
The issue is fixed in Control Expert version 15.1

The following information explains what was fixed to resolve the issue.

The fix for the issue involved two corrections:
  • The diagnostic parameter “NEW” which was not working as explained in the documentation.
  • One very specific use case was taken into account where the DFB S_RD_ETH_MX2 could update data into OUTPUT_SAFE_DATA with some data older than the one which was already existing (but still compliant with the SAFETY_CONTROL_TIMEOUT). However, these conditions could not appear in a normal condition system and could be revealed only by very specific conditions (insertion of corrupted and very specific time data)




Schneider Electric Saudi Arabia