{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to get and provide the Control-Expert’s application used by the PLC after an issue in PLC ?
1/  Open the application in Control-Expert and connect to the PLC by choosing "PLC->Connect" command or clicking on "Connect" iconconnect

2/ Check if the opened PLC application into Control-Expert is identical to the one stored into the PLC by checking if "Equal" is set into the status bar :equalIf Not "EQUAL", upload the application from the PLC to the PC in Control-Expert by choosing "PLC->Transfert Project from PLC" command or clicking on "Transfert Project from PLC" icon : upload cmdupload
Then, check that "EQUAL" status is set into the status bar.

3/ Provide the *.sta file available in the customer folder (or archive the application file in *.sta format)

Schneider Electric Saudi Arabia