{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
UPS firmware file transfer using Network Management Card web interface fails
Issue: UPS firmware file transfer using the Network Management Card (NMC) web interface fails

Product Line:
  • Smart-UPS models with a SmartSlot or embedded NMC.
Environment:
  • UPS systems with Network Management Card 2 (AP9630, AP9630CH, AP9631, AP9631CH, or embedded NMC2) firmware v.6.8.0 or higher:
  • UPS systems with Network Management Card 3 (AP9640, AP9641, AP9643, or embedded NMC3)

Cause: When performing the UPS firmware update using the NMC web interface, while connected to the web interface over WI-FI, a different network, or VPN, a file transfer timeout may occur if an HTTPS connection is used.

Resolution:

Option 1 (RECOMMENDED): The transfer timeout will not occur if the firmware transfer is performed over an SCP connection. Follow the steps outlined in FAQ000242942 to update the UPS firmware remotely using SCP and command line interface.

Option 2: The transfer timeout will not occur if the firmware transfer is performed over an HTTP connection, but this is not recommended due to lack of encryption.

Step 1: In the web interface of the NMC, enable HTTP in "Configuration", "Network", "Web", "Access", and select "Apply":
enableHTTP


Step 2: Reboot the NMC. This will not affect the load connected to the UPS.
Enable "Reboot Management Interface" in Navigate to "Control", "Network", "Reset/Reboot", and select "Apply":
rebootNMC

Confirm the reboot:
rebootNMC2

You will be logged off. Select Log On:
loginNMC


Step 3: Click the URL and manually change https to http. Press Enter.
URLedit


Step 4: Log in using your user name and password. Follow the steps outlined in FA170679 to update the firmware of your UPS.


Step 5: Once the firmware update has completed, HTTP access can now be disabled. Deselect HTTP in "Configuration", "Network", "Web", "Access", and select "Apply".

disableHTTP

Step 6: Refer to Step 2 to reboot the NMC.

Schneider Electric Saudi Arabia

UPS firmware file transfer using Network Management Card web interface fails
Issue: UPS firmware file transfer using the Network Management Card (NMC) web interface fails

Product Line:
  • Smart-UPS models with a SmartSlot or embedded NMC.
Environment:
  • UPS systems with Network Management Card 2 (AP9630, AP9630CH, AP9631, AP9631CH, or embedded NMC2) firmware v.6.8.0 or higher
  • UPS systems with Network Management Card 3 (AP9640, AP9641, AP9643, or embedded NMC3)

Cause: When performing the UPS firmware update using the NMC web interface, while connected to the web interface over WI-FI, a different network, or VPN, a file transfer timeout may occur if an HTTPS connection is used.

Resolution:

Option 1 (RECOMMENDED): The transfer timeout will not occur if the firmware transfer is performed over an SCP connection. Follow the steps outlined in FAQ000242942 to update the UPS firmware remotely using SCP and command line interface.

Option 2: The transfer timeout will not occur if the firmware transfer is performed over an HTTP connection, but this is not recommended due to lack of encryption.

Step 1: In the web interface of the NMC, enable HTTP in "Configuration", "Network", "Web", "Access", and select "Apply":
enableHTTP


Step 2: Reboot the NMC. This will not affect the load connected to the UPS.
Enable "Reboot Management Interface" in Navigate to "Control", "Network", "Reset/Reboot", and select "Apply":
rebootNMC

Confirm the reboot:
rebootNMC2

You will be logged off. Select Log On:
loginNMC


Step 3: Click the URL and manually change https to http. Press Enter.
URLedit


Step 4: Log in using your user name and password. Follow the steps outlined in FA170679 to update the firmware of your UPS.


Step 5: Once the firmware update has completed, HTTP access can now be disabled. Deselect HTTP in "Configuration", "Network", "Web", "Access", and select "Apply".

disableHTTP

Step 6: Refer to Step 2 to reboot the NMC.

Schneider Electric Saudi Arabia

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range:
move-arrow-top