{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PME2021 Installation Error with Driver Package TH110 / CL110
Issue:

During PME2021 Installation, the step "InstallUDFDrivers" is failing.

PME CL110

Root cause:

This is a known issue with non-English Operating Systems.

The following error can be seen on the Installation Log:
Install_log

Resolution:

If this is the only step that who failed, you can click on "close" button of the PME Installer.

Download and install the PME2021 Cumulative Update 1 (or more recent Cumulative Update).

The issue has been corrected in the PME 2021 CU1.

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: