{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I create an admin badge for EVlink Pro AC ?
From the factory there is no admin badge recorded.
At the first power on of the charging station, the first badge tapped on the RFID reader is recorded as an admin badge. In this case the charging station will blink once. If the charging station does not blink it means there is another admin badge already recorded.
To create or erase another admin badge you need to use the eSetup app.
When you use a admin badge it is confirmed by a green smooth pulsing of the LED during 1 minute

Schneider Electric Saudi Arabia