{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Importing Control Expert Classic project returns error 'The IO Scanning mode must be set to enhanced'
Importing a 'Control Expert Classic' project returns the following error:
error1


This occurred because the 'Control Expert Classic project' was not built using Control Expert 15.1 Classic with the I/O Scanning Mode set to Enhanced before creating the export file (.zef).  This is required because:
  • The I/O scanning mode cannot be changed after import.
  • The Topology Manager only supports Enhanced mode.

Use the following steps to set the IO Scanning mode to enhanced:
  • Open the project with Control Expert Classic 15.1.
  • Open the project settings.
  • Click on Build Settings.
  • Click on IO Scanning mode.
  • Select Enhanced from the drop down menu.
  • Click on Apply.
  • Save the changes.
  • Export the project as a '.zef'.
properties

Schneider Electric Saudi Arabia