{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the password used for the Zelio relay inside the enclosed ATV660 Drives?

Issue:

ATV660 enclosed Zelio relay password

Product Line:

ATV660, ATV960

Environment:

All

Cause:

Needs to access the password to look at the program or to change the program.

Resolution:

The default password for the Zelio relay is 6601 however according to the manufacturing plant some may have been shipped out with password 6101 and 6201.

Schneider Electric Saudi Arabia