Issue:
Customer wants to use the ATV630 at elevation over the maximum elevation listed in the Manual (1000 meters).
Product Line:
Altivar 600 series (ATV630, ATV650, ATV660, ATV680)
Altivar 900 series (ATV930, ATV950, ATV960, ATV980)
Environment:
Altitude over 1000 meters
Cause:
High elevation jobsite
Resolution:
See the following table for details on derating when used at high elevation.