{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you set up Brake Logic Control on a ATV930 drive?

Issue:

Setting up Brake Logic Control on a ATV930 drive.

Product Line:

ATV930

Environment:

Brake Logic Control

Cause:

n/a

Resolution:

Go to 5.9 menu (Hoisting Functions)

Brake Logic Control- set to R2

Movement type- Hoisting or Traveling

Brake Contact- set to the corresponding Digital input

Brake Relay Feedback- set to the corresponding Digital input

Brake release Pulse – set to yes or no or 2IBR

Brake release Current-current you want the brake to release

Brake Release Time- suggest around .5 secs

Brake release Freq- Auto

Brake engage freq-Auto

Brake engage delay-.00 secs

Brake engage time-time to engage the brake- suggest around .5 secs

Engage at reversal- No (if you do not want the brakes to engage in reverse)

Jump at reversal-auto

Time to rstart-.00 secs

Current ramp time-.00 sec

Schneider Electric Saudi Arabia