Search FAQs
How many Ethernet and Serial devices can be connected simultaneously to Com'X 510/210?
Answer
Issue
How many Ethernet and Serial devices can be connected simultaneously to Com'X 510/210?
_____________________________________________________________
Product Line
Com'X 510/210
_____________________________________________________________
Environment
Com'X Gateways
Modbus mastering
_____________________________________________________________
Solution
The Com’X supports up to 64 total devices which means Com'X will only log data for 64 devices, however Com'X has restriction even for Ethernet devices up to 32 as a maximum simultaneously TCP connections into gateway.
Therefore, if there are maximum 32 Ethernet Devices connected to Com'X, at the same time another maximum 32 Serial devices can be connected to reach the limit of 64 devices.
Based on standard, Com'X RS485 serial port supports up to 32 serial devices unless there is a signal repeater and Com'X has not reached the limit of 64 devices.
It is important to note that there is a difference between how many addresses that can be supported and how many devices that can truly be integrated. Performance of the Com’X clearly depends on how many complex devices are integrated and how often the information needs to be updated and published.
For critical applications less Modbus devices are recommended.
Issue
How many Ethernet and Serial devices can be connected simultaneously to Com'X 510/210?
_____________________________________________________________
Product Line
Com'X 510/210
_____________________________________________________________
Environment
Com'X Gateways
Modbus mastering
_____________________________________________________________
Solution
The Com’X supports up to 64 total devices which means Com'X will only log data for 64 devices, however Com'X has restriction even for Ethernet devices up to 32 as a maximum simultaneously TCP connections into gateway.
Therefore, if there are maximum 32 Ethernet Devices connected to Com'X, at the same time another maximum 32 Serial devices can be connected to reach the limit of 64 devices.
Based on standard, Com'X RS485 serial port supports up to 32 serial devices unless there is a signal repeater and Com'X has not reached the limit of 64 devices.
It is important to note that there is a difference between how many addresses that can be supported and how many devices that can truly be integrated. Performance of the Com’X clearly depends on how many complex devices are integrated and how often the information needs to be updated and published.
For critical applications less Modbus devices are recommended.
Released for:Schneider Electric Saudi Arabia
Explore more
Product:
Explore more
Product: