Issue:
Using a generic SD card with the HMIG3U HMI
Product Line:
HMIG3U, Vijeo Designer
Resolution:
You may use any generic SD memory card up to 32Gig formatted for FAT32. There are different speed class. No particular speed class is required, however the higher the class number the faster the speed. Class 10 is recommended for better performance.
Using a generic SD card with the HMIG3U HMI
Product Line:
HMIG3U, Vijeo Designer
Resolution:
You may use any generic SD memory card up to 32Gig formatted for FAT32. There are different speed class. No particular speed class is required, however the higher the class number the faster the speed. Class 10 is recommended for better performance.
Released for:Schneider Electric Saudi Arabia