{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: eConversion Live from the Lab 1: Efficiency Gain

eConversion is a patented high-efficiency mode for Schneider Electric Galaxy V Series (VS, VM, VL, VX) UPS that combines the best efficiency (up to 99%) with maximum load protection (IEC62040-3 class 1, VFI1.1.1 – equivalent to Double Conversion). eConversion typically provides a 3x reduction of the UPS electricity consumption. This live video from the lab shows an example of efficiency gain obtained when using eConversion. Discover more via eConversion Savings Calculator.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: