{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I Connect FDM128 Display to the EcoStruxure Panel Server ?

FDM128 and EcoStruxure Panel Server (all references) are compatible.

Data from PowerTag Sensors and Breakers (MasterPact, Compact and Acti 9) can be monitored on the FDM128.

Ensure to have the following Firmware baseline:

  • EcoStruxure Panel Server v001.003.001 or higher
  • FDM128 v08.00.30 or higher
For more update please refer to the:

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: