{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
New IP30 Option Kits for Easy UPS 3M



IP30 Option Kits for Easy UPS 3M are available for all IEC regions worldwide (except Japan):
SKUDescription
E3MOPT008EasyUPS 3M IP30 Kit for 60kVA-80kVA 400V UPS with internal batteries
E3MOPT009Easy UPS 3M IP30 Kit for 60kVA-100kVA 400V UPS for external batteries
E3MOPT010Easy UPS 3M IP30 Kit for 120kVA-160kVA 400V UPS for external batteries
E3MOPT011Easy UPS 3M IP30Kit for 200kVA 400V UPS for external batteries
By installing these option kits, Easy UPS 3M UPS can achieve the IP30 protection level against a solid object greater than 2.5mm (such as a holding tool or wires). Using the IP30 kits, the UPS will provide full load without any derating at 30°C, and the UPS power rating will derate to 85% of the nominal power rating at 40°C.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: