{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What can cause Overload relay to trip on ATV212 S-Flex?
Issue:
The currents are low and balanced but overload trips on S-Flex. Overload setting is good.

Product Line:
ATV212, S-Flex

Environment:
All

Cause:
NA

Resolution:
If using multiple motors on ATV212 or S-Flex drive, then try setting parameter Pt=0(Constant V/Hz).
Constant V/Hz is designed for running multiple motors at the same time(motors in parallel).

Schneider Electric Saudi Arabia