{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
SCADAPack x70 MB_SERIAL_MASTER Logic Editor Example
When using a SCADAPack x70 device it is recommended to use the Modbus Scanner implemented with RemoteConnect for simple Modbus polling of a server device (Modbus RTU or Modbus/TCP).

It may be desirable to have more control with the use of a logic program to perform the Modbus Client operations. An end user can use the MB_SERIAL_MASTER block in the logic editor to perform these tasks.

This example shows how to implement a typical Modbus read/write sequence in logic with retries and error detection. It uses a combination of LD (Ladder Logic) and FBD (Function Block Diagram) for section execution.

Schneider Electric Saudi Arabia

Attachment(s)
575_SerialMBusMaster.zip [187.91 KB]