Search FAQs
Testing your Geo SCADA application after an upgrade
Below are some common areas to test after an upgrade to a newer version of Geo SCADA takes place:
- The database server starts as expected, no errors occur during the start up
- The server’s license is being recognized
- The ViewX clients are licensed and connect to the database server as expected
- All outstations are able to communicate to their respective devices
- Data arrive as expected from the outstations
- Mimic navigation works as expected
- Mimic scripts are able to run without errors
- For redundant systems:
- All redundant servers are able to synchronize with the main server
- Server changeover works as expected
- For Virtual ViewX:
- Virtual ViewX server is upgraded as well as the rest of Geo SCADA
- Virtual ViewX clients are able to connect to the database server
- 3rd party clients are able to connect to Geo SCADA and perform their tasks
Released for:Schneider Electric Saudi Arabia
Explore more
Product:
Explore more
Product: