{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where can you find the ILF fault code number for the ATV320 Drive with an VW3A3616 Ethernet option card?

Issue:

Where can you find the ILF fault code number for the ATV320 Drive with an VW3A3616 Ethernet option card?

Product Line:

ATV320+VW3A3616 Option card

Environment:

All

Cause:

Need to ID which subcode is showing for the ILF fault.

Resolution:

Using the VW3A1101 HMI or the VW3A1111.

-Drives Menu

-Monitoring 1.2

-Diagnostics

-More Fault Info

Internal link fault: code number.

Example sub code 18= EEPROM detected error

ILF fault

Schneider Electric Saudi Arabia