{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
P3 programmable delay curve
Issue
We have a programmable delay curve function in our Easergy P3 relays, which function can let customer costomize a delay curve for overcurrent and earth fault protection and so on (based on current).
But our manual didn’t explain to our customer how to calculate the delay time if the fault current is between the setting points.
Take below picture as an example, if fault current is between 1A and 4A, customer is thinking this trip delay curve is linear, so customer think if fault current is 3A, trip time should be 8s, but actually our relay will trip after 8.235s.
Customer don’t know how to calculate the trip time, so they can’t verify our protectin function on site.
1

Product Line

Easergy P3 relay

Environment
All firmware version
Root Cause
The calculation of programmable delay curve is missed in our manual.

Solution
1- For temporary solution, please kindly find the attached PDF provided by R&D team, we can share this calculation document to our customer.
2- For permanent solution, it will be updated to the manual in future release.
Attachments/Links
Programmable delay curve explanation

Schneider Electric Saudi Arabia

Attachment(s)
Programmable delay curve explanation.pdf [128.42 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.