{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the DHCP name of BMENOS0300 located in remote rack ?

Issue:

What is the DHCP name of BMENOS0300 located in remote rack ?

Product Line:

M580

Environment:

EcoStruxure Control Expert

Resolution:

The DHCP name of BMENOS0300 is expressed as Cxxx_0y_BMENOS.


C002_06_BMENOS means it is loacted in the seventh slot (06) of a remote rack identified as CRA has rotary address 2


C105_04_BMENOS means it is loacted in the seventh slot (04) of a remote rack identified as CRA has rotary address 105


Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: