{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to show a video (.mp4) in the Web Visualization of EcoStruxure Machine Expert?

The WebVisualization of EcoStruxure Machine Expert can display videos by following these steps:

1) Create a new .html file. (Simply create a normal .txt file and rename the .txt extension to .html)

2) Copy the following content into the file and paste the filename of the video

<html>
<video controls="true" height="480" width="640"> 
<source src="video.mp4" type="video/mp4" /> 
</video>
</html>

3) Transfer the .mp4 and the .html file to the controller (under the folder visu). Important: The two files must be in the same directory.

4) Start the controller and open the webpage http: // <IP-Address>: 8080 / <Your HTML file name> .html or http: // <IP-Address>: 8080 / <Folder name> / <Your HTML file name> .html

Note:
The html file can be accessed directly via the link. It is not managed by the device user rights management.

Schneider Electric Saudi Arabia