{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What would cause the error "Topological address index is not valid" in EcoStruxure Control Expert after a build?
Issue:
"Topological address index is not valid" error in EcoStruxure Control Expert after a build


Product Line:
EcoStruxure Control Expert


Resolution:
The error occur when a variable is assigned to a memory object that is not allocated in the processor configuration. In the example below, the variable has an array length of 26 EBOOLs starting at %M500 to %M525. The processor memory management is configured for only 512 Ebools(%M). This is not enough to satisfy the array length. To clear the error, simply increase the %M to a number greater than 525 and rebuild the project.


image

Schneider Electric Saudi Arabia