{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ATS480 No Power Communication Error

Issue:

What is a No Power Communication error on a ATS480 soft start?

Product Line:

ATS480

Environment:

Fault code

Cause:

n/a

Resolution:

This fault is saying there is No Communication with the soft start while CL1 and CL2 are present.

Can power down the soft start and check all the inner connections.

Would also suggest to check the firmware version of the soft start.

This fault can occur if there is a hardwire failure with the soft start.

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: