{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I-line II busway be installed under a raised floor?

Issue:

Needs to install busway under a raised floor

Product Line:

Busway

Environment:

I-line II Busway

Cause:

N/A

Resolution:

Our I-Line II busway can be installed under "raised floors" as long as the busway joints and support system are accessible and the space is not used as return air systems.

Schneider Electric Saudi Arabia