{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How do I upgrade the firmware of the BMENUA0100 OPCUA server module?

Issue:
Firmware upgrade of the BMENUA0100 OPCUA server module


Product Line:
BMENUA0100, EcoStruxure Automation Device Maintenance


Resolution:
First log into the module via the web pages and go to the cyber security setup tab then select access control

image1

Create an account and select the appropriate roles for the user, "installer" necessary






image2

Apply the changes
image3

Launch the Automation Device Maintenance utility and select settings then package settings. The package location is where you copy the firmware file to
image5

The firmware should be available in the list under the data package
image6

Next, select Device/Loading tab and select Add
image7

Set the connection to HTTP/HTTPS and enter the IP address of the BMENUA0100 module then select ok
image8

Device should appear in the device list, make sure the data package reflect the firmware version you are upgrading to. Then select "Device Login" icon and enter the user credential of the module and select "connect"
image8b

The device login icon should turn green indicating a valid login. Next select the "Update Firmware" button at the bottom
image9


Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: