Search FAQs
What is the minimum mounting clearance free space for the front of the Size 6 ATV630 and 930 Drives?
Issue:
What is the minimum mounting free space in front of the Size 6 Drives?
Product Line:
Size 6 ATV630 and ATV930 Wall mount.
Environment:
All wall mount size 6 only
Cause:
Minimum front mounting size is 100mm.
Resolution:
100mm or greater are required for size 6 because it has ventilation openings in the front to have natural convection inside the electrical area.
This result comes from a thermal test during the validation phase of the project.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: