{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the current generated for a channel on the BMXAMO0410 for a 10VDC signal?

Issue
I am trying to determine voltage drop from a 2-10VDC signal generated by a BMXAMO0410 AO Module.
What is the current generated at the device to provide the 10VDC signal?

Product Line
X80 Analog I/O Modules - BMXAMO0410

Environment
Electrical characteristics

Resolution
For the BMXAMO0410, per channel, the minimum load impedance for voltage output is 1 kOhm.
Where the min load impedance is 1 kOhm, that means at +10VDC, the max current draw cannot exceed 10mA. 10vdc/1000 ohm= 10mA.

Also see: https://en.wikipedia.org/wiki/Output_impedance

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: