{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the embedded NMC capable of reading or detecting the AP9613 dry contact when inserted into the Smart slot of the UPS?
Issue: Clarification about the accessory board (AP9613) and the embedded NMC

Product line: All Smart UPS with Embedded NMC and available Smart slot

Answer:
No!
The embedded NMC cannot detect or read the dry contact AP9613.

An embedded NMC as well as the removable/preinstalled NMC can only detect a dry contact which is directly connected to its I/O  port.

Embedded NMC and AP9613 Dry Contact.JPG

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: