{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why do I see the OpcUaBase library in the Library Manager with the version number shown as "(not resolved)" for my M262 in EcoStruxure Machine Expert?

Issue
Why do I see the OpcUaBase library in the Library Manager with the version number shown as "(not resolved)" for my M262 in EcoStruxure Machine Expert?

For example, the TM262M15MESS8T is not supported and you would see the following "(not resolved)" in the Library Manager on the right pane (red box) below:
Library Manager - not resolved example

Product Line
EcoStruxure Machine Expert
Modicon M262 PLC

Cause
The most likely cause is that the model of PLC that you have added to your project does not support the OpcUaHandling or OpcUaBase libraries
that do support the OpcUaHandling and OpcUaBase libraries are limited to only these three models in the M262 lineup:

  • TM262L20MESE8T
  • TM262M25MESS8T
  • TM262M35MESS8T

(plus the LMC PacDrive family which are a different family for Motion control)

See Section "O" from this help doc which goes over the supported models: Libraries Overview (schneider-electric.com)

Supported Devices for OpcUaBase Library



Resolution
You will need to add one of the three supported models of M262 instead of the not compatible models.

Again, the three supported M262 models are:

  • TM262L20MESE8T
  • TM262M25MESS8T
  • TM262M35MESS8T

Schneider Electric Saudi Arabia