Search FAQs
Is the OFS Server V3.63 supported on Windows 11 operating system?
Issue:
OFS Server V3.63 supported on Windows 11 operating system
Product Line:
OFS server
Resolution:
Yes, but you will have to install SP2. Below is the link to download SP2 for the OFS server V3.63.
https://www.se.com/sa/en/download/document/OFS_3_63_4904_SP2/
OFS Server V3.63 supported on Windows 11 operating system
Product Line:
OFS server
Resolution:
Yes, but you will have to install SP2. Below is the link to download SP2 for the OFS server V3.63.
https://www.se.com/sa/en/download/document/OFS_3_63_4904_SP2/
Released for:Schneider Electric Saudi Arabia
Explore more
Product:
Explore more
Product: