{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How do I update the firmware of my SRTG 15 & 20kVA UPS?
Issue:

SRTG 15 & 20kVA UPS requires a firmware update.

Product Line:

Smart-UPS models SRTG15KXLI and SRTG20KXLI

Environment:
  • Computer with Windows 7 or Windows 10 operating system
  • The USB A to USB B type communication cable supplied with the UPS
  • "UPS-UpdateToolInstaller.zip" file - available at the end of this document
  • "15-20k V1.19 20220909.zip" Firmware File - available at the end of this document

Resolution:

NOTE: The UPS system is expected to power down during the firmware upgrade. It is recommended to turn off the load connected to the UPS before starting the firmware upgrade.

Preparation:
  1. Connect the USB A to USB B type communication cable supplied with the UPS cable between the UPS and computer. 
    • image.png
  2. Download the "UPS-UpdateToolInstaller.zip" and "15-20k V1.19 20220909.zip" files attached at the end of this document.
  3. Extract the "UPS-UpdateToolInstaller.zip" file.

Installing the Update Tool:

Double click the "UPS-UpdateToolInstaller.exe" file to start installing the update tool.
  1. Select OK.
    • image.png
  2. Select Next.
    • image.png
  3. Select Install.
    • image.png
  4. Ensure that the "Launch UPS-UpdateTool" option is selected, and then select Finish. This will launch the update tool.
    • image.png

Updating the UPS Firmware:
  1. Select the language: English.
    • image.png
  2. Select the appropriate port number where the USB cable is connected to the computer.
    • image.png
  3. Press "select" and browse to the location where the "15-20k V1.19 20220909.zip" file was downloaded in Preparation Step 2. 
    • image.png
    • image.png
  4. Ensure both check boxes are ticked:
    • image.png
  5. Select Updating:
    • image.png
  6. The update may take 15-20 minutes. Once the update is completed, the update tool can be closed:
    • image.png
Verifying the firmware version

Use the UPS front panel to navigate to the following menus.
  1. Press the OK key to enter the Main Menu, press the ▼ key to select Configuration and press the OK key to enter the submenu.
    • image.png
  2. Press the ▼ key to select Display, and click OK to enter the submenu.
    • image.png
  3. Press the ▼ key to select the Menu Type, and click OK to enter the menu type selection screen.
    • image.png
  4. Press ▼ key to select Advanced, and press OK to confirm.
    • image.png
  5. Press ESC key until you return to the Main Menu.
  6. In the Main Menu, press the ▼ key to select About, click OK to enter the submenu.
    • image.png
  7. Select UPS and click OK to enter the submenu.
    • ​​​​​​​image.png
  8. Press the ▼ key to view firmware component versions.
    • ​​​​​​​​​​​​​​image.png​​​​​​​
 

Schneider Electric Saudi Arabia

Attachment(s)
15-20k V1.19 20220909.zip [301.17 KB]
UPS-UpdateToolInstaller.zip [10.77 MB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.