{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the VW3A3721 Multi-Drive Link Communication module proprietary to Schneider Electric?
Issue:
Customer has asked if the VW3A3721 Multi Drive Link Communication module is proprietary?

Product Line:
ATV630, VW3A3721

Environment:
Ethernet IP

Cause:
n/a

Resolution:
Yes the VW3A3721 Multi Drive Link communication module is proprietary to Schneider Electric.
The code is based on Ethernet I/P protocol, but the exchange frames are internal to the Multi Drive Link communication module.


VW3A3721 Communication module
  • https://www.se.com/ww/en/product/VW3A3721/communication-module-ethernet-ip-modbustcp-multidrive-link-altivar-10-100mbps-2-x-rj45-connectors/

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: