Search FAQs
ATS480 Soft Starter power and motor cable terminal connections.
Issue:
Where are the main power and motor cables connected on the ATS480 soft stater?
Product Line:
ATS480 Soft Starter
Environment:
All
Cause:
Power and Motor terminal connections.
Resolution:
(L1 L2 L3) (A2 B2 C2) (T1 T2 T3) power and motor terminal connections.
L1 L2 L3 are the line voltage power terminals.
A2 B2 C2 are the optional shorting contactor terminals.
T1 T2 T3 are the motor cable wiring terminals.
Please refer to the most recent ATS480 installation manual NNZ85515 version 4 or higher for more additional information.
ATS480 user manual User guide | Schneider Electric
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: