{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can you read or access RSTP data over Ethernet on the ATV600 or ATV900 Process drives?

Issue:

Reading RSTP data over Ethernet on the ATV 600 and ATV900 Process drives.

Product Line:

ATV600 with VW3A3720 option card or ATV930 Drives.

Environment:

All

Cause:

Reading RSTP over serial communications.

Resolution:

ATV900 or ATV600 with Ethernet IP card are compatible with other RSTP devices (switch, PLC).

However, there is no way to read the RSTP status over the Ethernet network.

Schneider Electric Saudi Arabia