{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the ATV630 and ATV930 Profibus option card VW3A3607 feature both DPV0 and DPV1?

Issue:

ATV630 Profibus option card VW3A3607 features DP and DP V1?

Product Line:

ATV630 and ATV930 Profibus option card VW3A3607 only

Environment:

All

Cause:

Features DPV0 and DPV1

Resolution:

Yes, this profibus option card VW3A3607 does support both DPV0 and DPV1

Schneider Electric Saudi Arabia