Search FAQs
ATV6000 MV Drive support Ethernet TCP-IP and Ethernet IP?
Issue:
ATV6000 Embedded Ethernet support both Ethernet TCP-IP and IP?
Product Line:
ATV6000
Environment:
All
Cause:
Ethernet Commnications.
Resolution:
Yes, the Embedded Ethernet on the ATV6000 MV Drive does support both Ethernet IP and Ethernet IP.
Note this Ethernet port needs to be configured during the ATV6000 MV commissioning or start up.
Related information
ATV6000 Embedded Ethernet manual link
ATV6000 Ethernet Embedded Manual | Schneider Electric (se.com)
ATV6000 Communications parameters link
ATV600 - Communication parameters addresses Software - Released | Schneider Electric USA
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: