{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the maximum number of buffered events allowed in a SCADAPack x70 RTU (DNP3 and IEC-60870-5-104)?

In legacy SCADAPacks (SP32/Sp3xx) the maximum number of DNP3 events was ~20,000. This was SCADAPack programmed with Telepace or SCADAPack Workbench CAM3 firmware. The legacy SCADAPack E (3xxE 53xE) could retain ~40,000.

If a end user is using a SCADAPack x70 RTU AND firmware 9.8.6 or greater, the maximum buffered events can be configured for DNP3 and IEC-60870-5 104 are set at 100,000 events. The default is set to 5000 events. This is configured on the events tab in RemoteConnect.

Max Events

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: