{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Cannot login to PME web with error, "User is not licensed"

Issue

The following error occurs when the user tries to login into PME Web:
User is not licensed

Access denied. This user is not licensed for web access.

• The problem happened even when no other user was logged in PME Web.

• By default PME comes with 2 web licenses, included in Base License (applies to both PME 9.0 and above versions upto PME2023). In this case 2 additional web licenses were purchased, for a total of 4 licenses.


Product Line

Power Monitoring Expert (9.0, 2020, 2021, 2022 & 2023)

Notes:

  • The problem was observed in PME 9.0 but it could apply to other versions as well
  • The script (in resolution section) works in 9.0, 2020, 2021, 2022 & 2023


Environment

PME Web Application


Cause

Exceeding the number of PME Web licenses


Resolution

Database Warning: “This article contains information about editing the database. Please note, editing or updating anything in DB may cause permanent damage and result in PME to function improperly. This procedure should only be performed by users familiar with SQL Server Management Studio. Kindly take a backup of the database before performing any such action."

Licenses are assigned to users. In case there were previous users, the assigned license needs to be freed.

In order to achieve this run the following script:

delete FROM [ION_Network].[dbo].[GroupMembershipMap]

where TrusteeID NOT IN (SELECT UserID FROM [ION_Network].[dbo].[Users])

For convenience the script is attached to this article.

Schneider Electric Saudi Arabia