{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is It possible to view the free memory space of the BMENOP0300 module ?
It is possible to monitor the free dynamic memory space of the BMENOP0300 module. This feature is available on the module firmware version SV2.6 and higher, with the IEC61850 Configuration Tool V3.3 and higher:

BMENOP0300 firmware history

We can view the free dynamic memory space in the device DDT of the BMENOP0300 module:

BMENOP0300 Device DDT overview

Schneider Electric Saudi Arabia

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: