{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
There was a problem loading the Configuration Applications" in Web Applications

Issue
Web Applications will open and load but will throw the error "There was a problem loading the Configuration Applications". Unable to access any of the application tools.

Product Line
Power Monitoring Expert 7.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment
PME- Web Browser

Cause
Power Monitoring Expert leverages several ION services. A list of these services can be found here. ION Application Modules Provider Engine Host Service hosts web services that provide data processing for the Web Applications component and should be set to automatic. Without this service running, the Web Applications will not be able to access the necessary data to be used.

Resolution

  1. Navigate to C:\ProgramData\Microsoft\Windows\Start Menu\Programs\Administrative Tools. Select Windows Services.

  2. Set ION Application Modules Provider Engine Host Services by right-clicking the service, select Properties ,and select Automatic from the Startup Type menu. Press Start. Select OK.

  3. Return to PME web applications and refresh the page.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.