undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Can a Model 6 MCC be configured to 415VAC 50Hz voltage system?

 

415v 50hz is available for Model 6 MCC's as a special. We can issue special pricing for the application. Will have to know if there are any control power transformers or power supplies that will need to be converted.

Schneider Electric Saudi Arabia

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.