{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

PowerChute Network Shutdown reports “Error registering with the Network Management Card.”

Issue:
PowerChute reports “Error registering with the Network Management Card.”

Product:
PowerChute Network Shutdown version 4.x or 5.x

Environment:
PowerChute Virtual Machine
All supported Linux OS
All supported Windows OS

Cause:
Connection issue with the APC Network Management Card.

Solution:
Please review the attached PDF

For the PowerChute Virtual Machine and Linux systems, see:
"Error registering with the Network Management Card when running the PowerChute Virtual Machine or on a Linux system.pdf."

For PowerChute running on a Windows system, see:
"Error registering with the Network Management Card when running the PowerChute on a Windows System.pdf."

Schneider Electric Saudi Arabia

Attachment(s)

Error registering with the Network Management Card when running the PowerChute Virtual Machine or on a Linux system.pdfError registering with the Network Management Card when running the PowerChute Virtual Machine or on a Linux system.pdf [350.41 KB]
Error registering with the Network Management Card when running the PowerChute on a Windows System.pdfError registering with the Network Management Card when running the PowerChute on a Windows System.pdf [396.14 KB]
Explore more
Range:
PowerChute Network Shutdown
Explore more
Range:
PowerChute Network Shutdown
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.