{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
E3SOPT001 SSH CBC Detected
Issue: Detection of CBC (Cipher Block Chaining) ciphers being enabled in SSH, which can be flagged by vulnerability scanners

Environment:
E3SOPT001 Firmware 3.7.DA807.APC.19 and lower

Cause:
Vulnerability scanners detect CBC ciphers as a potential security vulnerability in SSH configurations, which is the cause of this issue.

Solution:
The SSH ciphers will be updated on future firmware release.  Please note that an exact ETA for the update is not available at this time. This FAQ will be updated accordingly.

Note: SSH uses the highest preference cipher that both the server and client support, which means it will prioritize the most secure cipher available.

If you have further questions or need additional information, please reach out to your local Customer Care Center. Check the link below and set the correct country.
How to Contact APC - APC USA

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: