Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Why is the boot up time longer on the ATS480, than the ATS48?

Issue:

Customer has a ATS480 and when it is powered up it shows “Welcome to Schneider” boot up screen. They state it takes about 8 seconds for the Soft start to boot up and 

it’s unacceptable for their process. Any way to reduce the start-up process? 

 

Product Line:

ATS480

 

Environment:

Boot up time

 

 

Cause:

n/a

 

Resolution:

The ATS480 have a software and hardware control that is different compared to ATS48.

After a power on of Control voltage (CL1-CL2), the starter needs about 6.5 secs for the wake up.

The reason the boot time is higher on ATS480:

The flash memory is larger and there is a increase in the time of the initialization of the file system.

ATS480 embeds a secure boot and the firmware integrity check time is significant.

Unfortunately, there is not a way to reduce this time.

 

Schneider Electric Saudi Arabia