{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Upgrade from 8.0 to 8.1 may not properly upload to the server / "Install Update" grayed out.
Issue:
Upgrade from 8.0 to 8.1 may not properly upload to the server / "Install Update" grayed out.

Product Line:
EcoStruxure Data Center Expert

Environment:
Upgrade from 8.0 to 8.1

Cause:
After attempting to import the DCE 8.1 upgrade from ithin DCE 8.0, you may not get the "Install Update" option as it may remain grayed out.

If you look in the Client log, you may also see an error similar to the following:
!ENTRY com.apc.isxc.logging 4 0 2023-12-21 10:17:04.272
!MESSAGE Failed to upload file: null
!STACK 0
java.io.IOException: Stream closed


This is due to a timeout in the HTTP configuration

Resolution:
This should only happen when uploading with a transfer speed of about 2mbps or less.

The solution is to connect using a client that is in the same network segment assuming that will increase network connectivity speed.

Schneider Electric Saudi Arabia

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.