{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to Invert the CT polarity of an ION Meter that does not have the Verification tab in the Setup Assistant
Issue
Some ION meters do not have the Verification tab in the Setup Assistance due to age making it difficult to understand how to change polarity of CTs

Product Line
ION metering
ION Setup


Environment
ION Setup

Resolution
The attached documents details the steps required to change the polarity of an ION meter

Schneider Electric Saudi Arabia

Attachment(s)
How to Invert the CT polarity of an ION Meter that does not have the Verification tab in the Setup Assistant (1).pdf [207.56 KB]