{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
NetBotz NBPD0165 camera may sustain damage if connected to incorrect NetBotz port
Issue:
NetBotz NBPD0165 camera may sustain damage if connected to incorrect NetBotz port

Product Line:
NetBotz version 5

Environment:
NBPD0165
NBWL0755
NBRK0750

Cause:
Although many ports on the NetBotz appliances use the RJ45 type connector, specific ports are designed to be used with different sensors or pods.

Resolution:
The NBPD0165 is specifically designed as a network camera requiring POE for power. The network ports on the NetBotz 750 and 755 appliances are specifically ethernet ports with power over ethernet (POE).
Other ports on the NetBotz appliance may have different voltages on different pins on the RJ45 connector and connecting sensors, pods, or cameras to ports not specifically designed for them can cause irreparable

Schneider Electric Saudi Arabia